Hi team,
I'm Jayden, I have some questions about enable and adjustable UVLO when I run the EVM in the lab.
The waveform on the left shows EN is float without RENT and RENB. Only the pullup current Ip sets the default state of the pin to enable. The waveform on the right shows EN with RENT and RENB. The pullup current Ip and Ih sets the state of the pin to enable.
1.Why there is a 1.18V voltage platform in EN when it is floated at start-up sequence?
2. Why there is a voltage slope change in BP5?
3. SW has a single pulse before Vout is established. It also occurs in datasheet Fig8-10. Why does this single pulse appear?
Thanks. Look forward to your reply.