Other Parts Discussed in Thread: LM25037
Hi guys,
I'm thinking about using the LM25037QMT to design a boost converter that would take a 12V input from my battery and convert it to a 24V output.
I want to use a topology of an H bridge so that I can have regenerative properties at the same time .My load being a motor ,sometimes it ends up being a generator so I also want my circuit to be able to charge my battery when this happens.
I'm thinking about using the LM25037EVAL as a reference design to design my converter, however there are certain things from this eval board I'm having a hard time understanding. Could you guys give me a little help with that?
Thanks a lot
- There is a part of the circuit I don't understand. It is the part containing the components C20,D5&L3. I've put a picture below. What is the purpose of this circuitry? From my little knowledge in converter, these components would not be required for a typical flyback.
- I'd like to use this eval board to do my first tests. What would I have to modify on the board so that it properly operates with a 12VDC input and give me a 24VDC output instead of the actual output of 5V?
- Are they any further considerations I should take when using the LM25037QMT as my controller of my h-bridge converter ?
Thanks a lot guys