This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25600: Vbus beyond 13.5V Condition

Part Number: BQ25600

I have a design using BQ25600. I noticed that the Vbus operating range is up to 13.5V. 

The datasheet noted that IC can handle up to 22V for an hour. 
But there is missing information about what will happen if a voltage is in the range of 13.5V-22V.  

If I have a power adapter with multiple outputs of 5V, 9V, 12V, and 15V, will that be a concern if the adapter somehow fails and outputs 15V? 

Thanks in advance for any insights. 
Simon