This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562211EVM: When Vin<6.45V, Ven<1.12V,the EVM will shutdown.

Part Number: TPS562211EVM

Vin‘s range is 4.2V-18V,This R1 R2 causes the circuit to shut down when the input is less than 6.45V.

Why choose such a resistance value for the R1,R2?