This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS2597EVM: TPS2597EVM

Part Number: TPS2597EVM
Other Parts Discussed in Thread: TPS25200, TPS25947

Hi,

I just want to understand what are the meaning of these parameters while choosing resistance.


Also, is there any e fuse available which can provide me following functions.

  1. OVER VOLTAGE PROTECTION (adjustable)
  2. OVER CURRENT PROTECTION(adjustable)
  3. REVERSE POLAIRTY PROTECTION

i am using TPS25970ARPWR right now but its minimum voltage is 2.7V while the system that i need to protect have following parameters.

Input voltage (2 x AAA batteries connected in series) i.e. 3V to 3.44

Input Current = 2100mAh

The minimum voltage should be at least 2.4V or less if possible.

Thanks