Hello,
I would like to ask you about the UCC27517DBVT device.
We are checking the short circuit between IN+(3pin) and GND(2pin) of this device.
(Question)
Will the device destroy if the attached waveform is applied between IN+ and GND?
Since the device has a resistance of HBM4kV, if the noise applied in the attached waveform is the cause of the device breakdown, is it more likely that it is insulation breakdown rather than thermal breakdown?
The waveform has a rise time of several nanoseconds, and the width of one pulse is as short as just under 20ns, so I don't think the amount of heat applied is as high as HBM4kV.
Best regards,