Dear Team,
If we just change the output voltage, do you need to adjust the value of code?
Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
Please refer to the VOUT_SCALE_LOOP command section of the datasheet (page 47) for the order for programming the output voltage upwards or downwards (not all commands may be necessary).
Hi Tomoya,
Thanks for your great support!
TPS544B25RVFR Apply for a new code, can you provide the code with the following specifications?
Requirement spec: vout=2.57, Itdc=6.6A , Imax=8.9A
Please help to double check the spec. Thanks.
Many Thanks,
Jimmy
Hello Jimmy,
Tomoya is OOO until the end of the week:
For 2.57Vout, the R_BIAS and R1 ration is 1:1 according to table 1 in DS and this what you selected.
Thanks!
Tahar
Hi Tahar,
Thanks for your great support!
Could you help to review schematic and share your comments with us(3.3V and 2.57V)?
Many Thanks,
Jimmy