Other Parts Discussed in Thread: TPS1211-Q1, TPS25940-Q1
Can TPS24720 be used in automotive and aerospace applications?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can TPS24720 be used in automotive and aerospace applications?
Hi Gary,
Welcome to E2E!
TPS24720 is not suitable.
Can you share voltage and current specs to suggest suitable part
BR,
Rakesh
Hi, the circuit that was used in the original thread TPS24720: schematic design review shows the voltage and current requirements. It was my colleague who asked for the schematic review.
I need an automotive version of TPS24720.
please see below
V1 = 5V @ 12A TPS1211-Q1
V2 = 3.3V @ 18A No Solution
V3 = 3.3V_Aux @ 6A TPS25940-Q1
Can we use TPS1HB08A-Q1? Our requirement is 3.3V @ 18A. The nominal supply voltage is 6-18 but the datasheet says "Extended supply voltage" is 3-28. What is extended supply voltage? How do we use this in a 3.3V application to limit the current to 18A?
Hi Gary,
I have looped in appropriate engineer to help on TPS1HB08A-Q1. He will get back
Hi Gary,
TPS1HB08 cannot be used in DC operation in the extended supply range. This range is meant for transients like cold crank condition.
Another major concern is the DC current as 18A is much larger than what the device is rated to handle.
Thanks,
Shreyas