I'm trying to get this 48V 2A boost stabilized. It starts to behave erratically and singing when the load approaches 1A, showing small/large pulses on the SW pin which would indicate sub harmonic oscillation. I've tried reducing Rslope to 90k with no improvement.
SW @ 300mA load
HO @ 300mA load:
LO @ 300mA:
Unstable operation @ 900mA load:
SW:
HO:
LO:
I've also noticed that the switching frequency is about 10KHz higher than it should be at the SYNCOUT pin. The Rt resistor is 37.4k (verified correct part is installed) which should yield a Fsw of 240kHz, but it's measured at 253kHz as shown here.
Any advice would be greatly appreciated.