Other Parts Discussed in Thread: TPS745
Hi,
I have the TPS745 used in the following manner.
After first power up, the Vfb was 0.567V (and the output 0.835V instead of 0.8V).
Which seems out of spec, though marginal.
Yet after several (10-20) power cycles the Vfb kept increasing till the output became equal Vin (1.78V).
Enable signal is driven by 1.8V open-drain buffer.
PG pull up voltage (V_3V3_MB) is up before Vin (V_1V8_MB).
Please advise what could be the reason for this failure.
Thanks,
David.