This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90160: UCD90160 and TPS65273V are not responding on PMBUS

Part Number: UCD90160
Other Parts Discussed in Thread: TPS65273V

Hi TI team,

I have built an evaluation board with 2xUCD90160, 3xTPS65273V for my project and debugging with TI tools

My first issue is devices are not responding on GUI

my board is referencing PMP9444 and provide power for FPGA and DRAM

I have set the UCD90160 address as 0x65'h and 0x66'h, one of TPS65273V address is 0x60'h on the same PMBUS

2x TPS65273V on another PMBUS with address 0x61'h and 0x62'h

However, only 0x62'h found ACK on GUI debug interface, all other devices cannot be found

I have checked the resistors are correct value. Or I remove UCD90160 ADDR0/1 resistor setting default address 126'd but still found no device

My second question is TPS65273V is hardware shutdown when start up, do they still respond to PMBUS?

can I pre-config its output value before enabling it?

I attached my project schematic for reference.

Thanks a lot.

UCD90160 and TPS65273V are not responding.pdf