Hi TI team,
I am using LM5156-Q1 boost converter and wanted to calculate the Line/load regulation of the converter, but with the available formula I think I am not getting the correct value. Also for switching regulators do we get such data in datasheets as a specification?
Vin = 5.7V to 6.3V; Vin_typ = 6V
Vout = 12V
Formula used are:
Line regulation = [delta Vout / delta Vin] x 100%
OR
Line regulation = ((delta Vout / Vout) x 100%) / (delta Vin)
And
Load Regulation = (V.No_Load - V.Full_Load)/(V.Full_Load) * 100%
Is this the right way to calculate the line/load regulation for boost converter?
Regards,
Sunney