Other Parts Discussed in Thread: TPS4811-Q1, LM74502,
Q1. Can you please share with me the details of D1, D4, D5, D6 and D7 diodes for example design 2 on page 27 in the datasheet? (the part number would be great)
Q2. This question seems it is a general question about MOSFETs but What is the important thing we are picking up a mosfet for the example design: LM5060EVAL Design. For example, my system requirements are like these:
Operating voltage range 14V to 24 V, Current max 13A , OVP setting 27 V typical UVLO setting 12 V typical.
So in that case, I try to keep Rdson res lowest value as much as possible when I am choosing a mosfet. Of course, Drain-source voltage and continuous drain current are always higher than the operation max voltage and continuous current. Basically, I am always confused about Gate-Threshold Voltage and rDS(on). Can you please clarify these points for me please with the examples? Is there any recommendation on what mosfet can fit my system?