Other Parts Discussed in Thread: LM5170EVM-BIDIR
Hello,
I have a question that I need this boost converter EVM module with 24V input. This 12V input port can be connected to 24V battery?
And the duty cycle is varying in this module?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I have a question that I need this boost converter EVM module with 24V input. This 12V input port can be connected to 24V battery?
And the duty cycle is varying in this module?
Thanks
Hi Muhammad,
Thank you for using E2E forums, the LM5170EVM-BIDIR's user guide as shown below specifies the maximum and minimum input voltage range of the BOOST mode operation:
As for the duty cycle, yes it is varying with maximum and minimum duty cycles depending on the design specifications.
BR,
Haroon