Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65580: Current consumption at no load

Part Number: TPS65580

Hello,

My customer is using the TPS65580 under the following conditions.

    - VIN=12V, VOUT=5V

1. What is the current consumption specification of TPS65580 when there is no output load?

2. As a result of measurement on the customer's board, the following deviations occurred for each board.

    - Bd #1 : 37mA / Bd #2 : 52mA / Bd #3 : 83mA / Bd#4 : 115mA / Bd #5 : 132mA

     Is this normal? What is the cause of this symptom?

Thank you.

JH