Hi, team!
There is a question about TPS7A16 voltage output drop.
We gave the TPS7A16 an input voltage of 6V and expected output voltage was 3.3V, but the output voltage only remained for about one second, then dropped(input voltage was still 6V). Input current is about 1.15mA when it works normally.
I took a photo about output voltage. The blue is output voltage(2V/div) and Input current is green but it's too small to test. Others are not used.
You can see that the output voltage was about 3.3V at first, then skipped to 5V and dropped to 2V finally.
So I think current was not the reason to cause voltage drop. So could you explain the cause of the phenomenon?