This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08080W to Power Iridium 9602 Unit

Expert 1070 points
Other Parts Discussed in Thread: PTH08080W, PTN78020W, PTH08T231W

Hello,

We are considering using your PTH08080W module to power the Iridium 9602 satellite transciever.  The power supply requirements for the Iridiums are:

(11 to 15 VDC Input, 5VDC 2A output)

1) Droop for 8.3ms burst of 1.5A current should not be more than 0.2Volts.

2) In-rush current to Iridium limited to 4A maximum.

Will this module do the job?  Can you recommend this part or is there another that might be better?  This is a battery operated system so efficiency is important.

Thanks.

Loren