I need to produce +5V @ 60mA and -5V @ 20 mA from 15V.
The loads are not symmetrical so direct split-rail generation with a coupled inductor (http://www.ti.com/lit/htm/slva369) is not an option, or is it ?
A plan would be to use one TPS62120 for 15V -> 5V, and a second one for 5V -> -5V.
So I'd like to know if it's possible to use the TPS62120 to produce negative voltages ?