Because of the holidays, TI E2E™ design support forum responses will be delayed from Dec. 25 through Jan. 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629210EVM: TPS629210EVM

Part Number: TPS629210EVM
Other Parts Discussed in Thread: TPS629210

Hello! 
I am trying to get the TPS629210 on TPS629210 evaluation module to output 3.45V .
I have used the formula indicated to the datasheet (page20), and Replaced R2 with 32.4K .
The configuration Jumpers are to the default position. 
The problem is that I am only getting 2.5V as output. 
I have tried this with two different kits and the result is the same. 
According to the datasheet it should be possible to get 3.45V.
Is there any other component that needs to be changed? 
Is it possible that the default configuration of the kit is not valid for 3.45V operation?