Part Number: TPS61178
Hi,
We are using TPS61178RNWR boost converter in one of our design. I have attached an schematic for boost converter which we have design. Please review the schematic and provide your feedback.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TPS61178
Hi,
We are using TPS61178RNWR boost converter in one of our design. I have attached an schematic for boost converter which we have design. Please review the schematic and provide your feedback.
Hi Sonali,
From your schematic, I find some points might need to be checked.
1. the input voltage and current range. Note that there is a remark that the current is 0.8A, I guess the BAT need average current limit to be 0.8A ,right?
the current limit resistor should be checked to meet the lowest input voltage to ensure 0.8A current limit.
2. the voltage reference is 1.198 typically, so after voltage drop the output shall be nearly 12.5V. Please confirm your demand.
3. the compensation resistor and capacity is recommended to be lower value, like 15Kohm and 6800pF.
Best Regards
Fergus
Hello Fergus,
Sorry for the late reply.
1. The 0.8A current is at lowest input voltage i.e. 10.8V. Can you please tell us what should be current limit resistor value for 0.8?
Also, we have used 86.6k limit value to limit current upto 8A peak current.
2. The input voltage (VBAT) is 10.8V to 12.6V and we need boost output voltage upto 12.8V for our application. It is possible to do this?
3. Okay, we will changed compensation to lower value.
Thanks,
Sonali
Hi Sonali,
1. it can be calculated that the ripple current is around 1A at 10.8V input, so your peak current is 0.8/2+1=1.4A,
you can use 3A current limit that the resistor can be 250k.
2. it is possible to do this. but the chip's current may be too large for the application.
Thanks,
Fergus
Hello Fergus,
Thank you for your feedback.
1. Where do you find the formula (0.8/2+1=1.4A) which you have used to calculate peak current.
Thanks,
Sonali
Hi Sonali,
Sorry I wrote the wrong formula.
The frequency is around 500kHz (the Rfreq=316k) and the duty is 1-Vin/Vo=0.163
The current ripple Δi=Vin*d*Ts/L=1.07A.
The right formula is

We get the peak current formula Ipk=0.8+1/2=1.3A.
Best Regards
Fergus