Other Parts Discussed in Thread: LM76002
Hi team,
quick question regarding the minimum input voltage that the LM76003 needs to keep the output voltage stable.
Example: 24V supply (VIN = 25-48V, VOUT = 24, P=50W)
Following the first page of the d/s, we could only guarantee Vout = 95% * VIN, however, the min duty cycle in the electrical specs is mentioned to be 97.5%.
- Can the device support VIN = 25V & VOUT= 24V?
- What is the reason / cause to have the VOUT limitation? Is it the duty cycle or smth else?
Thanks and best regards
Martin