This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62933: audible noise

Part Number: TPS62933

Hi team,

customer load is a PWM step load which has a frequency ranging from 60Hz~20kHz,

with normal TPS62933,the audible noise is obvious.

I try to add 10ohm dummy load (10V, 1A), to boost up the switching frequency to above 100KHz at low side ( no load sinking)

but the noise is still hearable , as you can see below.

does this mean even OOA version can't solve this also? 

since I notice the bottleneck is not the low switching frequency , but the frequency of  Fsw variation