This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS1641: Min and Max of Operting Supply curent (Vcc) and OUTPUT CURRENT LIMITING (ILIM)

Part Number: TPS1641

Hi experts,

Could you please tell me the minimum value and maximum value of ”Operting Supply curent (Vcc)” and  ”OUTPUT CURRENT LIMITING (ILIM)”?

On the datasheet, only the TYP value corresponding to the RLIM setting value is listed, but I think that the value may differ depending on the individual difference of the IC itself and the surrounding environment.

Best Regards,

Taito Takemura

  • Hi Taito Takemura,

    Vcc range is

    2.7V to 60V for TPS16412, TPS16413

    4.5V to 60V for TPS16410, TPS16411

    We are yet to determine the min and max for ILIM. Those data will be available during RTM in Dec-2022

    Best Regards,

    Rakesh