Hi,
I have a 48V 3phase motor controller in production that is having thermal issues (Bus Capacitors Poping).
My team has isolated the root cause of this failure to 2 circuits, both of these circuits are 48V, protected with individual TPS26600 chips and should have an over-current limit of 1.1A.
The chips have the following setup:
- Vin = 48V Lion Battery (38V-54.6V)
- CIn = 1uF (100V)
- In1, In2, UVLO connected
- UVLO to OVP 1.37MOhm
- OVP to RTN = 20KOhm (55v)
- DVDT to RTN = 47nF
- Mode not Connected
- ILIM to Return = 11K (around 1.1A)
- IMON = Not Connected
- SHDN = Not Connected
- FLT = Not connected
- Out 1 & 2 connected together.
Please note there is no Cout, Is this an Issue?
Are there any issues with this circuit layout?
Kind Regards
Tom