Other Parts Discussed in Thread: UCC21750
Hello,
As per UCC21750-Q1 datasheet, the DESAT detection threshold is typically at 9.15V.
I am using SiC MOSFET with 20mΩ RDS ON resistance. Considering peak current of 57A, series diode drop of 0.7V & series resistor drop of say 2V, the total voltage comes to be 3.84V (57*0.02+0.7+2).
This is far less than the threshold of 9.15V.
How this DESAT protection will help to prevent short circuit / overcurrent condition in this case?
As there is no pull-up value mentioned, can you please suggest how to calculate blanking capacitor & series resistor value?
Regards,
Abhishek Deshmukh