I need to use DCV010505D to supply ±5V to a amplifier.
I set the Vs=5V.
When there's no load , +Vout=+11.82V and -Vout=-11.78V.
When the amplifier is connected, +Vout=5.17V and -Vout=-7.82V.
Neither of them is ±5V as the expectation. I was wondering whether it's because the output of DCV010505D is unregulated as the datasheet says.
I want to get stable ±5V output from DCV010505D, how should I design the extern circuit?
Thank you!