I have some questions/problems regarding to TPS7A39 regulator. According to the datasheet, VNR/SS Internal reference voltage is between1.17V and 1.208V.
But I measured on my board, it is 4.4V (IC batch 1) and 1V (IC batch 2). I am not sure what is the problem.
I had use it in the previous layout (different batch of ICs), everything seems fine. I copied the same circuit, the IC didn't regulate properly as expected.
Instead of 6V and -1V as their output voltages, they output 11V and -11V almost same as the input voltage.
The two ICs built with different batch were tested in the same se-tup.