Hi All,
I have a question about the LM3478.
My customer is designing a circuit that can step-up and step-down. The customer has designed the following circuit based on a simulation circuit on webench.
This circuit may not work correctly. It will not work if the load current is changed.
VIN=6V
VOUT=24V
It also does not work correctly when it is operated under the following conditions.
VIN=38V
VOUT=24V
What are the possible causes?
In the webench simulation, VIN=6-38V / VOUT=24V / IOUT=0.1A.
Best Regards,
Ishiwata