Dear TI colleagues,
We are using LM5150-Q1 for electronic brake system application.
For this application, I have designed switching frequency 499.34kHz using RT=44.1kOhm(1% tolerance).
But measured frequency is slightly lower than calculated value in real circuit.
-Measured switching frequency : 484.2~484.94kHz in tri temperature conditions(-40, 25, 120 degree celsius)
-Measured voltage on RT pin : 1.133V
-Measured resistance of RT in real circuit : 44.1kOhm(Nearly)
My questions are
1) Measured frequency(484.2~484.94kHz) is no problem considering RT value and RT voltage?
2) When RT value is fixed, is there switching frequency tolerance? If yes, please let me know how much tolerance exists.
3) Voltage on RT pin is related to switching frequency? and there is any voltage tolerance on RT pin?