Hi,
I tested efficiency of TPS54202HEVM and found some suspicious efficiency. Below is the test data, and suspicious efficiency marked yellow. The test condition is Vin=6/12/18/24V, Vo=5V, Io=0.5/1/1.5/2A.
I have tried to find what's the problem. So I tested the SW node voltage, the cause of high efficiency when Vin=24V, Io=0.5A is that converter enter eco-mode and lose some drive signal, see below picture. But in datasheet Iskip=300mA, so can you tell me why converter enter eco-mode in this condition.
Finally, about the suspicious efficiency when Vin=6V and load current is large, I don't know what's the problem. The SW node voltage is normal.