Hello together,
we will have to connect /CE pin on our design and are asking if it is possible to connect via C3 and C4 (both NC pads). The datasheet says "C4 may be shorted to /LP" and for C3 " Do not connect to a any voltage source or signal to avoid higher quiescent current".
- Is C4 short only possible to /LP?
- Is there a rough estimate of how much the quiescent current increases if we would also short /CE to C3?
We have to balance between higher PCB cost or increased quiescent current.
Thanks in advance and best regards,
Marc