Other Parts Discussed in Thread: TPS23730, TPS23731EVM-095, TPS23731
Hi team
I have design question of PMP22477.
If the power limit is type 3, may I reduce this circuit? as shown below
I think it about current sense (CS), right? (the circuit application is?)
I do some testing on EVB which remove resistance (R33/R18/R52) and add resistance (R51/C46) and modify R67(0.05 to 0.015).
The transformer sound gets louder as the load increases.(The output is below 12W, and the transformer has no any sound)
Increase AUX current of the transformer can improve?
Have any suggestion to this ?
thanks
B.R
Zen