Other Parts Discussed in Thread: LM63460-Q1
Hi experts:
Can TPSM63606 support output 1.8V@6A with 12V input?
I am searching for a solution to regulate 12V input to the output 1.8V@6A, 2.5V@6A, 3.3V@6A, 5V@6A, 7.5V@6A, 8V@6A, 10V@6A.
Can TPSM63606 work for this?
Thanks,
Marsh