Hello Ti team,
in the datasheet chapter 7.5 , there are three Feedback voltage accuracy at different TEST CONDITIONS, but i can't find the Feedback voltage accuracy at "force PWM, VIN ≥ VOUT + 1 V, VOUT > 1.0 V, Co,eff ≥ 15 µF, L = 0.47µH " in my design, VIN=3.3V VOUT=1.2V, and set to force PWM mode . Does the force PWM and PWM mode share the same Feedback voltage accuracy ±1%? many thanks