Other Parts Discussed in Thread: TPS62130
Dear all,
Regarding TPS62130A, please tell me the minimum value of VH for EN pin.
In section 7.5 of the TPS62130A data sheet (REVISED NOVEMBER 2021), the minimum value of the EN pin is min 0.9V.
However, this is incorrect and I think the min value should be less than the typ value of 0.65V.
I checked with TPS62130EVM. TPS62130 is enabled when EN pin is 0.66V, and output voltage is output. So typ value 0.65V is reasonable.
(Attached is the waveform observed in EVM. CH3: Output Voltage (3.3V), CH4: EN Terminal Voltage (0.66V))
Please tell me the correct EN pin VH minimum value.
Best regards,