power IC low power mode fail record.xlsx
dear
customer use TLV70233 in Mass production stage,1000 out of 6000pcs have problem.Is there any design risk in sch,can you help to check sch and debug report?
thanks in advance
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
power IC low power mode fail record.xlsx
dear
customer use TLV70233 in Mass production stage,1000 out of 6000pcs have problem.Is there any design risk in sch,can you help to check sch and debug report?
thanks in advance
Hi Raymond,
I apologize for the delayed response. Thank you for sharing this information.
Has there been any change in the PCB design?
Also, have the PCB boards been cleaned thoroughly? Often times there might still be some resin or other residue from assembly. Make sure that the boards are highly cleaned.
Also, in your schematics, it shows that TLV702 has the following pin out:
Pin1: Vin
Pin2: GND
Pin3: CS
Pin4: BY
Pin5: Vout
However, the SOT-23 version has the following Pin out:
The circuit itself is ok electrically speaking.
Furthermore, I see that there is a BJT, has this been verified to properly working as well? is it possible to remove the BJT and possibly R109 and either keep R108 or solder short R108 to create a direct connection from EN to VIN to measure the current consumption?
Best,
Edgar Acosta