Hi, I do have a couple of question with the e-switch TPS26400:
1- Does the SHDN signal when driven can operated with respect to the RTN pin? and or with GND pin
2- Not clear for me what is the difference voltage between the GND pin and the RTN pin when IC operated normally (so not under reverse bias situation)
3- I do see a series resistor of 100Kohms between IMON and TP_IMON (TP5) on the EVM schematic (Figure 3-1) . Can you tell me more about the utility of this resistor please?
4- Finally, what could be the highest resistor suitable between pin IMON and RTN for the current monitoring? Does a 200K can be used in order to get a reliable/repeatable current monitoring value?
Thank you!
Regards
Bruno