Hello,
Greetings!!
We are using bq27531-G1 in our project. In our case, gauge has learned cycle count 'n' numbers (e.g. Cycle count =10), but when we insert new battery in the device the cycle count didn't change to " 0 ". The device shows the previous cycle count and SOH value.
Gas gauge will not sense that new battery has inserted and change the cycle count to 0 automatically? or we have to put " 0 " manually in the golden image file when the new battery is inserted?
As per TRM, The gauge maintains a separate cycle count for both cell profiles and resets to 0 if the insertion of a new pack is detected (page no. 17) but when we performed a test it's not resets to "0".
Regards,
Janhavi Rane