Other Parts Discussed in Thread: LMR33630, , LMR51430
To whom it may concern, my company uses TI part LM53603AMPWPR (or WPT suffix) to generate a 5 V supply for a load of up to 2.6 A and another almost identical circuit on the same PCA, to generate a 3.3 V supply for a load of up to 3 A.
This part is out of stock at the moment.
Other than the automotive version (LM53603-Q1 which is also out of stock), can you please recommend any drop in alternatives in an HTSSOP 16 package.
Note, I have looked at the LM63635DQPWPRQ1 and it is almost a drop-in replacement, but it is also out of stock.
Kind regards,
-Sebastien A.