This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS629203: What does dynamic mode change mean?

Part Number: TPS629203

Dear experts, as shown in the attached Table 8-1, what does dynamic mode change mean? If the current of my system during sleep is 20uA, and the current during operation is 20mA, considering the efficiency at light load, the 27.4K ohm setting of MODE/S-CONF pin is the best way? But at this time, dynamic mode change is not active, what does it mean? Best regards.