TPS65070 datasheet claims on page 33 "Depending on the sequencing option, the signal at EN_DCDC1, EN_DCDC2 and EN_DCDC3 are ignored. For automatic internal sequencing, the enable signals which are not used should be connected to GND". What happens if I connect them to high level?
More specifically, I need to turn some DCDCs on and off while system operating, and I do not care of predefined automatic power up/down sequencing. I beleive if I connect pins EN_DCDC2 and EN_DCDC3 to GND it won't be possible to control the DCDCs after changing DCDC_SQ[0:2] to 101. Is there a way to resolve that issue?
I would not like to use TPS65073 because of its DCDCs current ratings.