The datasheet does not state how the exposed pad (underside) is electrically connected. Is it possible to connect this pad to GND (same as DAP, SGND, RTN)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The datasheet does not state how the exposed pad (underside) is electrically connected. Is it possible to connect this pad to GND (same as DAP, SGND, RTN)?
Hello,
Please see below from the Layout Guidelines section:
The exposed pad on the IC package bottom should be soldered to a ground plane, and that plane should both extend from beneath the IC, and be connected to exposed ground plane on the board’s other side using as many vias as possible. The exposed pad is internally connected to the IC substrate. The use of wide PC board traces at the pins, where possible, can help conduct heat away from the IC. The four no connect pins on the HTSSOP package are not electrically connected to any part of the IC, and may be connected to ground plane to help dissipate heat from the package.
Regards,
Harrison Overturf