Other Parts Discussed in Thread: LM5175QUICKSTART-CALC, LM5175, LM5122
Hi there,
we are using the LM5175EVM-HP evaluation board for 12V output but now we would like to switch the output to be 18V. Looking at LM5175EVM-HP schematics it looks like the FB pin is connected to a voltage dividors with R11, R14, R22 that configures the 12V output. If adjusting this voltage resistors dividers it should be able to configure for 18V output?
Do you confirm we can change the voltage divider to get 18V output (or other output voltage) ?
Best, Javier.