This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM63615-Q1: Transient Pulse 1B

Part Number: LM63615-Q1
Other Parts Discussed in Thread: LMR36520

Hi,

Good Day.

As the customer is using the LM63615DQPWPRQ1 in our design, they are testing it for Transient Pulse 1B as per the ISO 6737-2, so the maximum voltage will have appeared across the device is 43.5V for 2ms - after every 5s for 500 repetitive pulses.  

As the maximum absolute rating of the device is 40V, so can device withstand the Pulse 1B of 43.5V for 2ms. Can you please specify the behavior?

Please advise. Thank you very much.

Best Regards,

Ray Vincent