Hi
My question is regarding the TPS7A4700, datasheet rev SBVS204F. I am getting most of the DC parameters to pass in my testing with the exception of the following fails ---> overall_accuracy and current limit at Vin/Ven = 3V. If Vin/Ven are increased to ~8V both tests pass. This has been verified on ATE and bench setup.
Any thoughts what could be causing these fails?
Thanks,
Joey
Low Limit Result High Limit Status
1 5 1 overall_accuracy VOUT VIN=3V IO=0mA 1.365000 V 1.400656 1.435000 V Pass
1 5 2 overall_accuracy VIN=3V IO=0mA -2.500000 % -0.046842 2.500000 % Pass
1 5 3 overall_accuracy VOUT VIN=35V IO=0mA 1.365000 V 1.402013 1.435000 V Pass
1 5 4 overall_accuracy VIN=35V IO=0mA -2.500000 % -0.143774 2.500000 % Pass
1 5 5 overall_accuracy VOUT VIN=3V IO=1A 1.365000 V 0.002806 1.435000 V Fail <------
1 5 6 overall_accuracy VIN=3V IO=1A -2.500000 % 99.799601 2.500000 % Fail <------
1 5 7 overall_accuracy VOUT VIN=35V IO=1A 1.365000 V 1.396264 1.435000 V Pass
1 5 8 overall_accuracy VIN=35V IO=1A -2.500000 % 0.266875 2.500000 % Pass
1 10 1 current_limit ICL 1.000000 A 0.388500 2.000000 A Fail <-----