This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27542-G1: Can not write the srec-file.

Part Number: BQ27542-G1
Other Parts Discussed in Thread: BQSTUDIO

こんにちは。

EV2300 を使用して .srec ファイルを BQ27542-G1 に書き込もうとします。
しかし、私は.srecファイルを書くことはできません、以下のコメントが表示されます。
"データ フラッシュ チェックサム計算された srec が、プログラミング後にデバイスから返されたチェックサムと一致しません。

私の会社の同僚は、「0542_2_01-bq27542G1.bqzファイルが古い可能性があります」と言います。
だから、私に最新の0542_2_01-bq27542G1.bqzファイルを送ってください。

そして、この問題について、解決策を知っていますか?
ご存知の方は教えてください。

感謝。

  • Translated:

    Hello.

    Attempt to write a .srec file to BQ27542-G1 using EV2300.
    But I can't write a .srec file, the following comments appear.
    "The data flash checksum calculated srec does not match the checksum returned by the device after programming.

    A colleague in my company says, "the 0542_2_01-bq27542G1.bqz file may be out of date."
    So please send me the latest 0542_2_01-bq27542G1.bqz file.

    And about this problem, do you know the solution?
    If you know, please let me know.

    Thanks.

    Hello Takashi,

    The bqz file on the webpage should be the most recent and correspond to the firmware you have, if BQStudio autodetects the device that means you have the correct bqz file.

    Usually with the checksum not matching it is related to the gauge not having a good power source, or bad communication so some of the transaction do not complete properly.

    Sincerely,

    Wyatt Keller