Other Parts Discussed in Thread: LMR36520
Hi team,
Could TPSM63603 used for 24V to -12V @1A application? if not, could you give some suggestions here?
Thanks a lot.
Matthew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Matthew:
we don't recommend use TPSM63603 is this spec, as for IBB, the max voltage will be Vin+abs(Vo) which is 36V in this condition, it is nearly no margin right now. we recommend a 60V 2A module or converter working at this condition.
for module, you can choose TPSM5601R5Hx, and make sure rated Io lower than 0.8A(1A may over its internal high side rated current which is 1.5A). For converter, LMR36520 will be recommend.
Thanks
Daniel Li