Dear team,
If these two pins ASC_EN & ASC are not used, they should be connected to GND with pulldown resistors in my understanding, right? What is the recommendation for the pulldown resistor? Is it ok to use 1kohm?
Thanks & Best Regards,
Sherry
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear team,
If these two pins ASC_EN & ASC are not used, they should be connected to GND with pulldown resistors in my understanding, right? What is the recommendation for the pulldown resistor? Is it ok to use 1kohm?
Thanks & Best Regards,
Sherry
Hello Sherry,
Our expert on this device is out of office today. he should be able to reply tomorrow.
Thanks,
Alex M.
ASC_EN and ASC should be well connected to ground if they are not in use.
Even if they are used we still recommend a pulldown resistor to ensure the logic state is low if the MCU outputs are highZ.
If the ASC and ASC_EN inputs are completely unused I recommend using a smaller resistor, even a 0 Ohm resistor, to directly tie the ASC and ASC_EN inputs to GND. THe prevents any possible noise coupling on the pins.
Regards,
Daniel