Hello,
I'm trying to configure some LGPO pins on the UCD90320. Sometimes the software gets into a state where any changes I make to the logic don't take effect in the device once I "Write to hardware" and "Store RAM to FLASH". If I click "Refresh all Parameters", I suddenly find two instances of an LGPIO with different configurations, see below where pin L4 appears twice:
In the above image, L4 is at the top and bottom of the list with a different configuration for each instance
I'm running Version 7.7.1 of TI Fusion Digital Power Designer.
I cannot be confident that the project's configured logic is being correctly implemented in the sequencer. Are you aware of this issue?