Other Parts Discussed in Thread: LM25149
Hi team,
I am designing LM25149 dual phase circuit. Could you please help answer my questions below?
#1. When Active EMI filter is not in use, how should I terminate them? NC is OK?
#2. RRT=9.52kohm Switching frequency 2 doesn’t match Equation (3) below.
The typical frequency should be 2.1MHz at RRT=9.52kohm.
Could you please confirm?
#3. I cannot use high resistance like 100kohm for pull up due to condensation risk.
Pull up of EXTCOMP(5pin) and PG pull up can be 10kohm?
How much is the minimum value?
#4. Detail behavior of adaptive dead-time methodology to prevent cross conduction.
regards,